For the business and trade press
Siemens announces second major wind turbine order in the U.S. within one week
Erlangen, Germany, April 03, 2008
Siemens Energy has been awarded another major order for a wind farm in the U.S. with a capacity of nearly 325 megawatts (MW). Siemens will supply 141 units of its 2.3-megawatt turbines for the Biglow Canyon Wind Farm Phases 2 and 3 in Sherman County in Oregon. The purchaser is Portland General Electric Company (PGE), a fully integrated utility that serves more than 804,000 customers in Oregon. This is the second major wind order from the Pacific Northwest that Siemens has publicized within one week. On Monday, March 31, the German-based company announced an order for 130 wind turbines that would produce nearly 300 MW in Washington State. The combined value of the two orders totals more than USD1.1 billion.
The Biglow Canyon Wind Farm Phases 2 and 3 will produce enough power to meet the electricity demand of approximately 100,000 households. Phase 2 of the project is scheduled to be operational in late 2009, and Phase 3 is expected to be on line in late 2010. The Siemens scope of supply consists of delivery, installation and commissioning of the 141 SWT-2.3-93 wind turbines with a capacity of 2.3 MW each, including a five-year warranty and separate service and maintenance agreement.
“Wind power is a rapidly growing source of electricity in the U.S. and the two major orders from Washington and Oregon will strengthen our position as one of the leading suppliers to the world’s largest market for wind turbines,” stated Andreas Nauen, head of Siemens’ wind business. “With nearly 1,000 MW installed or under contract in the Pacific Northwest alone, Siemens is helping to meet the growing demand for clean electricity in one of the most dynamic regions for wind power development in the world.”
The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2007 (ended September 30, based on IFRS), the Energy Sector had revenues of approximately EUR20 billion and received new orders totaling around EUR28 billion and posted a profit of EUR1.8 billion. The Energy Sector had a work force of 73,500 at the beginning of fiscal 2008. Further information is available at: www.siemens.com/energy.
All figures represent the sum of the nonconsolidated figures for the Power Generation and Power Transmission and Distribution Groups and for the Oil, Gas and Marine Solutions Division of the Industrial Solutions and Services Group.
Reference Number: ERE200804.019 e