Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

For the trade press


Siemens constructs Germany’s first commercial shoreside power supply system for ships berthed in port

Erlangen, Germany, May 20, 2008

Siemens Energy is installing a shoreside power system on behalf of the Lübeck municipal utilities on the Nordland dock. The system will provide ships with an environment-friendly and economical electrical power supply via the local medium voltage system while they are berthed in port. The first customer for the shoreside power system is the Finnish shipping line Transatlantic. The shipping company has already had the port of Kemi in northern Finland equipped with a system of this type. In June 2008, the three paper ferries Transpaper, Transpulp and Transtimber will be able to be supplied with electrical power from the shore-based supply at the destination ports of Kemi and Lübeck.

“As soon as the ships obtain the power they need via our shoreside power supply system, they can switch off their diesel generators while they’re berthed in port. These diesel generators not only produce electrical power but also exhaust emissions, soot, particulate matters and noise, so in this way these ships will help to reduce “harbor smog” which is becoming an increasingly serious environmental problem in many port cities,” said Ralf Christian, CEO of the Power Distribution Division in the Siemens Energy Sector.


The Transatlantic ships with their 400-V/50-Hz on-board systems have already been retrofitted for the Finnish shoreside power system and have a cable drum with plug-in connector, a control system for the coupling process and a transformer on board. In Lübeck, Siemens is installing the matching connecting point on the dock and creating the connection to the medium voltage network of the Lübeck municipal utilities. For this purpose, the company is installing a 10-kV switchgear for connection to the utilities and a 6-kV switchgear for connection to the on-board system. A cast-resin insulated transformer rated at 2500 kVA is also being installed in a concrete substation on the harbor site for separating the two networks electrically. Another component of the shoreside connection is a smaller concrete substation with a 6-kV outlet at its side enabling power to be obtained from the dockside via the plug-in connector of the ship.


The Lübeck shoreside power supply system operates at 50 Hz only because the on-board system of the ships uses the same frequency as the local power supply network. However, about 80 percent of the ships cruising the world’s oceans are equipped with a 60-Hz on-board system. If these ships are to be supplied with shoreside power, the frequency would have to be adapted. For this purpose, Siemens has developed the cold ironing system Siharbor, which enables on-board systems of ships and power supply systems on land to be connected together despite different voltages and frequencies.


The core element of this shoreside power supply system is the Siplink system developed by Siemens (Siemens Multifunctional Powerlink), in which two converters are connected together by a DC link and are each connected to one power supply network. In this way, Siplink can not only feed a separate network from a distribution network but can connect power supply systems with different parameters and interconnect them. Both these capabilities are used in the Siharbor solution as a means of linking the ship’s on-board system to the local power supply network.


In order to use the Siemens solution, both the harbor and the ship must be specially equipped for the shoreside power supply, among other things with a plug-in connection system. After connecting the plug-in connector of the ship, the automation system installed on shore can automatically initiate the start up of the shoreside power supply system. The user dialog for this is conducted from the ship. The ship’s power supply is not interrupted. Siplink is self-synchronizing and takes over the power supply within a few minutes. The diesel generators of the on-board power supply can then be shut down and the complete on-board network is supplied in an environmentally friendly way from the shore side power supply system.

 
 

The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2007 (ended September 30, based on IFRS), the Energy Sector had revenues of approximately EUR20 billion and received new orders totaling around EUR28 billion and posted a profit of EUR1.8 billion. The Energy Sector had a work force of 73,500 at the beginning of fiscal 2008. Further information is available at: www.siemens.com/energy.

All figures represent the sum of the non-consolidated figures for the Power Generation and Power Transmission and Distribution Groups and for the Oil and Gas activities of the Industrial Solutions and Services Group.

Reference Number: EPD200805.038 e

Press Contact

Dietrich Biester 
P.O. Box 3220
91050 Erlangen

Phone: +49-9131-7-33559

Fax: +49-9131-7-33615

dietrich.biester@siemens.com


Footer

Context Zone

Dialogue & Service

Service & Support


Related informations