Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

For the trade press


Power plant I&C system SPPA-T3000 now available as Release 4.0

Erlangen, Germany, February 18, 2008

The Siemens Energy Sector now offers for its world-leader I&C system SPPA-T3000 a Release 4.0 with extended functionalities, which go significantly beyond pure power plant I&C. Features such as mechanical equipment protection, thermodynamic system monitoring and a power plant simulator for training operating personnel can be fully integrated. A standard graphic user interface for a wide variety of applications is thus ensured. The plant operator’s hardware and maintenance costs are also reduced as well as costs for personnel training. With immediate effect the system will also be offered with a French and Chinese user interface in addition to German and English.

SPPA-T3000 is a web-based power plant I&C system which can be integrated seamlessly into the existing IT landscape of a power company and which is capable of providing real-time information for a wide variety of users. With its Embedded Component Services technology it simplifies power plant operation and maintenance, and thanks to its intuitive technology is precisely tailored to the needs of power plant personnel. It also enables plant operators to run individual power plant units in a flexible operating mode exactly matching the demand. Since it was launched in 2005, more than 220 SPPA-T3000 systems have been sold worldwide and the system is now being installed in all new Siemens power plants. “With Release 4.0 we are once again demonstrating our competence in the field of power plant I&C,” said Karlheinz Springer, head of Instrumentation & Controls at Siemens Energy, Fossil Power Generation Division. “With the new functionalities the system offers intelligent, cost-efficient solutions for all types of power plants. Siemens is thus expanding its leading position in this field,” added Springer.


 
 

The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2007 (ended September 30, based on IFRS), the Energy Sector had revenues of approximately EUR20 billion and received new orders totaling around EUR28 billion and posted a profit of EUR1.8 billion. The Energy Sector had a work force of 73,500 at the beginning of fiscal 2008. Further information is available at: www.siemens.com/energy

All figures represent the sum of the nonconsolidated figures for the Power Generation and Power Transmission and Distribution Groups and for the Oil, Gas and Marine Solutions Division of the Industrial Solutions and Services Group.

Reference Number: EFP200802.009 e

Press Contact

Gerda  Gottschick 
P.O. Box 32 20
91050 Erlangen

Phone: +49-9131 18-85753

Fax: -7039

gerda.gottschick@siemens.com


Footer

Context Zone

Dialogue & Service

Service & Support


Related informations