Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

Press Pictures Energy - IGCC / Gasification

IGCC (Integrated Gasification Combined Cycle) is an innovative technology for environment-friendly power generation. In addition to power generation the gasification of fuels such as coal, oil and refinery residues can also be utilized to produce valuable syngas, which can serve as the basis for the production of hydrogen, methanol, diesel fuel and a wide variety of other chemical products.


Coal gasifier

May 29. 2008

The Siemens coal gasifiers, which are 18 meters lo...

Gasification plant Vresová

Jan 01. 2006

The photo shows the upstream gasification plant su...

IGCC Puertollano

Jun 01. 1997

The photo shows the combined-cycle power (CCPP) pl...

IGCC Puertollano

Jun 01. 1997

The photo shows the combined-cycle power (CCPP) pl...

IGCC Puertollano

Jun 01. 1997

The photo shows the combined cycle power plant wit...

IGCC Puertollano

Jun 01. 1997

The photo shows the combined-cycle power plant wit...


Footer

Context Zone

Dialogue & Service

Service & Support


Related informations