Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

Raw Gas Injection

Gas produced from a well can be re-injected into the reservoir. One of the main reasons to do so is if the gas contains so many sour components (H2S, CO2) that it makes no sense to export the gas to other destinations, and flaring is not permitted. Re-injection of the gas into the reservoir can also increase the oil production. To enable gas re-injection, a compressor is needed to boost the gas pressure.
The required gas pressure depends on the pressure and depth of the field. Typically, the pressure is between 200 and 300 bar (2,900 - 4,500 psi) but for extreme cases, it can go up to 800 bar (11,500 psi).



Siemens contributes with:


Compression solutions


Drives



 
 

Footer

Context Zone

Dialogue & Service

Service & Support


Related informations